STM32CubeIDE (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

1.4.0 Bug? General Registers not updated debugging STM32F7

Debugging an STM32F7, the General Registers are not updated during dissassembly stepping.When clicking on one of the register values, as if to edit it, the real updated value does appear, but reverts to show the old value when no longer selected. Th...

EdGi by Associate III
  • 451 Views
  • 5 replies
  • 0 kudos

Resolved! Errors in STM32CubeIDE firmware update offline.

Hi,I have a problem with STM32CubeIDE firmware update. STM32CubeIDE wants me to download stm32cube firmware f7_v1.16.0. I downloaded manually this update file offline because of the system have no internet connection. I moved the whole STM32CubeFW-F...

AK47 by Associate II
  • 4129 Views
  • 6 replies
  • 1 kudos

Still fighting to setup SWO trace on STM32H7

Hello,A few months ago I tried without success to setup ITM on a STM32H753I-EVAL2 board (and STM32CubeIDE). Now I'm trying again. There is a precise point I'm not sure about: the signal SWO is multiplexed on GPIO PB3, so I have to setup PB3 with alte...

Gpeti by Senior II
  • 2093 Views
  • 29 replies
  • 0 kudos

NUCLEO-F756ZG ethernet CubeIDE configuration

Hello all!help needed! For last week I try to make UDP server on NUCLEO-F756ZG.I am stuck in the beginning...I can't configure my board to ping it.From reading old threads I understand that there was an issue with automatic ethernet configuration of ...

AKhar.5 by Associate II
  • 843 Views
  • 5 replies
  • 0 kudos