User Activity

Hy,I have tried to resample a 16bit/8kHz audio signal to 16kHz and 48kHz.Conversion works, but the audio is noisy. I am tested it on development board STM32H747 CM7 core.I have tried libraries: SRC236_CM7_GCC.a and SRC236HQ_CM7_GCC.a without quality ...
I am trying to run AcousticBF (Beamforming library v3.1.0 from XCUBE_SMARTMIC_V2.4.0 pack) on STM32H747 development board, but on the output I get only a tone signal, and no audio hearable from Mics. - The inputs are two PDM mics, and the PDM signal ...
I know that the library X-CUBE-AUDIO is not compatible with H7 series (only F4 and F7 is supported), but it can be very useful on the H7 mcu, too.Is there any way to make it run on the H747 cpu on M7 core?I want to use mainly SVC (SmartVolume) functi...
Hello, I trying to trace audio signal by SWV Data Trace Timeline graph? I cant do it. I can show normally only 10Hz signal. Higher frequency signals make a mismatch in timeline graph. I m using STM32F769 mcu, with coreClock: 216Mhz, SWO Clock: 2000kH...