STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1671 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 627 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

When trying to flash my program, I get an error Log that I do not understand, and that I can't find any information about online

when trying to flash my program, i get this error:Error in final launch sequence:   Failed to execute MI command: load >>Path<<\\Debug\\>>project_name<<.elf   Error message from debugger back end: Load failed Failed to execute MI command: load >>Pat...

Ubus99 by Associate III
  • 1649 Views
  • 3 replies
  • 0 kudos

HAL_QSPI_Transmit_DMA transfer limited to 20 us approx.

I send quad data via QSPI. But Transfer is limited to 20 us approx.At QSPI clock 25 MHz is possible send maximally 240 bytes (480 nibbles).At clock 12.5 MHz is possible send maximally 120 bytes.At clock 50 MHz is possible send maximally 480 bytes.I w...

DMato.1 by Associate II
  • 793 Views
  • 0 replies
  • 0 kudos

STM32H743VIT6 + STM32CubeIDE 1.4.1 + QSPI W25Q256

I am using the attached code, To access W25Q256 in QSPI mode,In the QSPI_ResetMemory ()Always returns QSPI_NOT_SUPPORTEDRunning this same code in STM32F765VIT6, it works.Analyzing the pins of the QSPI, I see no changes.

RDos by Associate II
  • 2238 Views
  • 3 replies
  • 0 kudos

Why this pity code at line 13 couse the Hard Fault?

#include "stm32f0xx.h" void SysInit(void);   uint8_t array1[260] = {0}; uint8_t array2[260] = {0}; uint16_t test; int main(void) { SysInit(); for(uint16_t i = 0; i < 260; i++) array1[i] = i & 0xFF; test = *(uint16_t*)&array1[0xEA]; test = *(uin...

MPony.1 by Associate
  • 3606 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.