STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32H743VIT6 + STM32CubeIDE 1.4.1 + QSPI W25Q256

I am using the attached code, To access W25Q256 in QSPI mode,In the QSPI_ResetMemory ()Always returns QSPI_NOT_SUPPORTEDRunning this same code in STM32F765VIT6, it works.Analyzing the pins of the QSPI, I see no changes.

RDos by Associate II
  • 2128 Views
  • 3 replies
  • 0 kudos

Why this pity code at line 13 couse the Hard Fault?

#include "stm32f0xx.h" void SysInit(void);   uint8_t array1[260] = {0}; uint8_t array2[260] = {0}; uint16_t test; int main(void) { SysInit(); for(uint16_t i = 0; i < 260; i++) array1[i] = i & 0xFF; test = *(uint16_t*)&array1[0xEA]; test = *(uin...

MPony.1 by Associate
  • 3429 Views
  • 8 replies
  • 0 kudos

"StringOut" works while "printf" doesn't.

Hello,I'm working with the NUCLEO-F722ZE EVB on STM32CubeIDE.In my code I tried to make the "printf" function work.I used the procedure described in this video:https://www.youtube.com/watch?v=9ntZ3dwGsMkIt basically involves adding this code (the ful...

skon.1 by Senior
  • 2317 Views
  • 5 replies
  • 0 kudos

Two CubeIde instances with two Debugger

Hello all,I have a SPI project: One Nucleo Board = SPI Master, Another Nucleo = Slave.I want to debug both boards (onboard STLink) at the same time by running two instances of CubeIde.Problem: both STLink listening to the same port on my PC. When one...

OBorg.1 by Associate III
  • 2168 Views
  • 2 replies
  • 1 kudos

Resolved! How to update CubeIDE from 1.3.0 to 1.3.1 instead of 1.4.1

Hi,all my co-workers work with CubeIDE 1.3.1 (with embedded MX 6.5.1). Because we share our projects I want to install the same version of IDE and MX.I already install CubeIDE 1.3.0 (which i found on ST site) and try to update it to 1.3.1.But only ve...

grzeslawm by Associate II
  • 2173 Views
  • 4 replies
  • 1 kudos