cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE, FreeRTOS, L082 device: CMSIS-RTOS v2 disabled?

RAltm
Senior

Hi,

I wanted to start learning FreeRTOS. I'm working with a L082 device, using CubeIDE. In the config file, I only can select CMSIS-RTOS v1 interface, v2 is disabled. But there's no explanation why.

So, I don't know if the device is unsupported by v2 or if there's something missing. I assume I can get it to work with v1, but...

Regards

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
KnarfB
Super User

> So, I don't know if the device is unsupported by v2 or if there's something missing. I assume I can get it to work with v1, but...

When you hoover the mouse over CMSIS_V2 is lists the supported series. L0 is not among them.

View solution in original post

2 REPLIES 2
KnarfB
Super User

> So, I don't know if the device is unsupported by v2 or if there's something missing. I assume I can get it to work with v1, but...

When you hoover the mouse over CMSIS_V2 is lists the supported series. L0 is not among them.

RAltm
Senior

Ah, okay. Thank you. Sometimes it's not clear if an option is disabled because of missing settings or because the device doesn't support it. Now it's clear.

Regards