STM32CubeIDE (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 1.17.0 released

We are pleased to announce to you that the release 1.17.0 of STM32CubeIDE is available. What is new in 1.17.0: Microcontrollers, microprocessors, and board lists aligned with STM32CubeMX: Added the support for the STM32N6 seriesAdded the support for ...

Multiple MCU support in a static library project

Some time ago I created a static library project in AC6 System Workbench for STM32. The project expanded and I started to adding build targets for more microcontrollers, STM32L, STM32F7, etc. After migrating the project to Cube IDE I am no longer abl...

0690X000009k2OhQAI.png
MMatu by Associate III
  • 368 Views
  • 0 replies
  • 0 kudos

Resolved! With the ADC using single ended input channel, what is the internal vref, what is the 12 bit voltage range for measurement (is it 0 to 2.5V or 0 to 3.3V)? What is the lowest accurate measurement resolution when we have less than 20mV to measure?

I am trying to work with photo diodes and need to measure 20mV or less with ADC. Whats the best resolution I can get with a single ended ADC (using ADC 3 channel 12 at the moment).Whats the measurement range on that channel? When we have less than 10...

PRedd.111 by Associate III
  • 480 Views
  • 2 replies
  • 0 kudos

Question about redefinition

Hi all,just a short question:Why does the compiler say that the page is redefined?#define ADDR_FLASH_PAGE_148 ((uint32_t)0x0804A000) #define ADDR_FLASH_PAGE_149 ((uint32_t)0x0804A800)Same page but with small letters and that's ok for the compiler...

eschl by Associate
  • 1041 Views
  • 4 replies
  • 0 kudos

Open in new window => STM32CubeMX view get's corrupted

Hi,I'm working with multiple monitors. I had to compare two STM32CubeMX files from two projects in the project tree. So, I right-clicked on one project, selected 'open in new window', and then openend the corresponding STM32CubeMX file. Both views of...

RAltm by Senior
  • 374 Views
  • 0 replies
  • 0 kudos

Problems debugging from STM32CubeIDE and Linux Debian

Hello developers,I am a beginner in STM32 programming.I have the board STM32L152C-Discovery, the ST-Link V2 adapter and Linux Debian on my laptop installed.I am using STM32CubeIDE as IDE.I setup my first project in STM32CubeIDE with the automated cod...

MHof by Associate II
  • 2375 Views
  • 8 replies
  • 0 kudos