Problems debugging from STM32CubeIDE and Linux Debian
- September 28, 2019
- 7 replies
- 3595 views
Hello developers,
I am a beginner in STM32 programming.
I have the board STM32L152C-Discovery, the ST-Link V2 adapter and Linux Debian on my laptop installed.
I am using STM32CubeIDE as IDE.
I setup my first project in STM32CubeIDE with the automated code generation and added my own code for toggling LED 4, which is being connected to Pin 7 of the CPU.
I can build and compile the project, but not debug it. Following error comes:
Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-06-12-13:05)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
none separate
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 8000 kHz
adapter_nsrst_delay: 100
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 1800 kHz
Error: init mode failed (unable to connect to the target)
in procedure 'init'
in procedure 'ocd_bouncer'
I am using the OCD debugger.
What can be wrong? Did I maybe have connected the wiring from ST-LINK-V2-adapter to the SWD pins of the board in a wrong way?
I also removed the jumper bridge from CN3 as described for debugging an external application. Did I forget something? Or do I have to change a solder bridge (if so, this would be stupid, because I do not have a soldering iron).
I have pictures of the wiring attached.
Many thanks in advance for your help!
Sincerely,
Marco