STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 564 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CAN initialisation error in Cube IDE using CubeMX 6.1.0

When trying to initialise any of the two CAN interfaces of my STM32F446RE in CubeMX, using the CubeIDE-integrated version, presumably a rounding error occurs.These are my settings:Prescaler: 5Time Quanta in Bit Segment 1: 6 TimesTime Quanta in Bit Se...

LSiew.1 by Associate
  • 3982 Views
  • 7 replies
  • 0 kudos

malloc(1)

I'm using cJSON on a STM32F401 and I'm a bit worried with possible problems regarding with memory allocation.If a call malloc(1) (so asking the heap for 1 byte only) how many bytes are really used on the Heap?I would assume correct answer with be 16 ...

EGonc.1 by Associate II
  • 2835 Views
  • 3 replies
  • 0 kudos