STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 564 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Adding existing source files to project

We are porting an existing vxWorks project to STM32. I am able to import the existing source files into a STM project, but I cannot get it to compile any of the files.I have tried a variety of project types and always refresh the project after addin...

RHerm.3 by Associate III
  • 3451 Views
  • 3 replies
  • 0 kudos

Long timer interrupt periods

Hello,I would like to have timer interrupts every 10 minutes for temperature readings. Also, I would like to have opportunity to change this period in the code. How could such long period be implemented? Are there any examples? I am using STM32L011F4...

Indois by Associate II
  • 6783 Views
  • 11 replies
  • 0 kudos

Resolved! Hello, Problem with new firmware version FW_F7 V1.16.1

When i open my .ioc file a popup windows appears with"this project was setup using STM32Cube firmware version FW_F7 V1.16.0 then new STM32Cube V6.2.1 works best with ...."I've tried the two options "continue" and "update" after that i have the follow...

SCAYL.1 by Associate
  • 2233 Views
  • 2 replies
  • 0 kudos