STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1433 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Question about overclocking STM32F411 in STM32CubeIDE

Hello I am working on a one off project that I would like to squeeze every last bit of power out of a STM32F411. I tried to overclock it just by increasing the clock speeds in the clock configuration section of cubeIDE but it always crashes when I tr...

CStew.2 by Associate II
  • 4021 Views
  • 9 replies
  • 0 kudos

how to make 2 headers in stm32cubeide include each other?

Hello guys!I am now using stm32cubeide and the issue is that there are 2 headers and I need them to include each other but when I do that, the compiler indicates that my typedef struct defined in a header is conflicting types. I have used this prepro...

TNguy.30 by Associate
  • 5041 Views
  • 4 replies
  • 0 kudos

I am not able to compile the code with STM32CUBEIDE 1.6.1 whereas I am able to compile the same project with STM32CUBE IDE 1.4.1. I am using STM32H7 HW.

Here is error details:GNU ld (GNU Tools for STM32 9-2020-q2-update.20201001-1621) 2.34.0.20200428 Supported emulations:  armelfc:\st\stm32cubeide_1.6.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.w...

ACHOU.18 by ST Employee
  • 1159 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L4R9I-EVAL examples do not show up in target selector

I am running v1.6.1 of STM32CubeIDE.When target selector is run using File/New/STM32 Project it does not list any examples for STM32L4R9I-EVAL even though I can find them in the L4 repository.I ran Update TTarget Selector DB and no change.Is it possi...

RHerm.3 by Associate III
  • 1393 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeIDE (project importer) 1.6.0 Works well?

Hello.I upgraded STM32CubeIDE from 1.5.0 to 1.6.0.But, in my environment, STM32CubeIDE (project importer).exe doesn't work well.As a work-around, I executed same program of 1.5.0 and it works well.Does it work in other (language) environment?- OS: Wi...

BLUEnLIVE by Associate II
  • 2140 Views
  • 5 replies
  • 0 kudos