cancel
Showing results for 
Search instead for 
Did you mean: 

.ioc file open in STM32CubeIDE 1.2.1

Dmitri
Associate II

After updating to STM32CubeIDE 1.2.1 I cannot open anymore .ioc file in STM32CubeMX device configuration tool. When I double click on existing .ioc in the project text editor opens instead of STM32CubeMX.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Julien D
ST Employee

Hi Dmitri,

I didn't faced it after updating to 1.2.1, the Device Configuration Tool is well opened when I double-click on the .ioc from the Project Explorer view.

You may have associated such file extension with another editor "by mistake".

In any cases it should be possible to use it back with right-click on .ioc, then Open With > Device Configuration Tool.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Julien D
ST Employee

Hi Dmitri,

I didn't faced it after updating to 1.2.1, the Device Configuration Tool is well opened when I double-click on the .ioc from the Project Explorer view.

You may have associated such file extension with another editor "by mistake".

In any cases it should be possible to use it back with right-click on .ioc, then Open With > Device Configuration Tool.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Dmitri
Associate II

"Open With" allows to start Device Configuration Tool. Thanks.

After I started build .ioc file icon changed to blue MX and file association was restored.

dbgarasiya
Senior II

is your .ioc file name and project name is same or not?

Yes. I use the same name for the project and .ioc file.

dbgarasiya
Senior II

solved ?

EDamm.1
Associate II

Thanks a lot,

I did not knöw this .ioc becausee I am a beginner with stm32cubeide.​