STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1433 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F746G-DISCOVERY, STM32CubeIDE, FLASH

Hello! While writing a program for writing data to FLASH, communication with DISCO is disabled. It cannot be recreated. DISCO is unusable. Can you protect yourself against it? greetingsAndrzej

How to make LwIP work with CMSIS_V2 in CubeIDE?

Hi,I have a Nucleo-F439ZI board and I am trying to make a simple application that echoes back a message on a UDP port.When I generate a project using LwIP raw API, I am able to make that happen with a callback function and a PCB.However, as soon as I...

GFeke.1 by Associate
  • 1766 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F746G-DISCO, STM32CubeIDE

I want to write to FLASH and read. Why doesn't it record?HAL_FLASH_Unlock(); FLASH_Erase_Sector(FLASH_SECTOR_7, VOLTAGE_RANGE_3); HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, FLASH_SECTOR_7, 300); HAL_FLASH_Lock(); set_time = *(__uint32_t*) FLASH_SECTOR...

Cannot install stm32cube_fw_f4_v1261.zip Error downloading files: (Target directory already exists). Multi year stm32cube bug is still not fixed. Updated previously documented workaround method for this particular firmware update. ARG!

This error message is false since the zip file downloads but errors during extraction.The folder inside stm32cube_fw_f4_v1261.zip is STM32Cube_FW_F4_V1.26.0 which I had already manually installed.So I guessed and changed the subfolder name for v1261 ...

Resolved! Issues setting up Ethernet/LWIP on STM32H753 (STM32CubeIDE)

Hello! I'm trying to run a LWIP example intended for another micro on the STM32H753 but ran into some issues setting up the H753 in STM32CubeIDE. In order to use LWIP, I'm getting this error:Ok, no problem. I went over to setup the Ethernet and it ap...

0693W00000BbvuYQAR.jpg
JayDev by Senior II
  • 1984 Views
  • 1 replies
  • 0 kudos