STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 564 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

I generated a simple project with STM32CubeMX When I compile that project I get: make: *** [Src/subdir.mk:27: Src/main.o] Error 3 "make all" terminated with exit code 2. Build might be incomplete.

I have the foll. settings:Properties...C/C++ Build...Tool Chain Editor...Current toolchain: Cross GCCProperties...C/C++ Build...Environment...PATH: C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.make.win32_1.1.0....

DNeet.1 by Associate II
  • 1611 Views
  • 3 replies
  • 0 kudos

How to change the FDCAN speed with parameter in CubeIDE?

I want to change the CAN speed with changed parameter which is defined in rom.c file. SY_CANBD = 1. But the FDCAN(Classic CAN mode) do not send the defined CAN data. If I starts the debugging mode, it starts to transmit the data. /* FDCAN2 init funct...

otcagon by Associate II
  • 1083 Views
  • 0 replies
  • 0 kudos

debug CubeIDE

Hello,I made a software on the STM32F469-Disco and now, I would like to use the same project on the STM32F479VI with the MB1166 (touch screen). If I create a new project, no problem, I can flash the microcontroller. If I start from the software made ...

RFREN.1 by Associate II
  • 3748 Views
  • 5 replies
  • 0 kudos

Resolved! Getting "Error: Target not available" in Value column in live expressions in StmcubeIDE in debug mode when i press Resume(F8)

I created a simple GPIO program with the code generated from StmCubeMX. When i build the program there are no errors and warnings, but when i connect my Nucleo-F411RE and try to debug it, i get this message in Expressions.The program is supposed to m...

0693W00000DnuFCQAZ.png 0693W00000DnuEsQAJ.png

Resolved! How to correctly uninstall and reinstall the stm32cubeide?

Hi,(1) Is it ok to install the IDE as my user and not via sudo? It seemed to be ok until I had some later issues which I wont go into here just yet as almost certainly "user error".(2) I installed the ide (as user), and because it was saying it could...

rileyrg by Associate II
  • 14904 Views
  • 2 replies
  • 2 kudos

I keep on running into -> void HardFault_Handler(void); When my HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *) pwmData, index); Is called

Hi. I seem to get HardFault_Handler error when I start my HAL_TIM_PWM_start_DMA function.I am not sure if it just gets stuck in an infinite loop in the while() called right after it.This looks like allot of code but really its just 5 of my functions ...

CMcC.1 by Associate II
  • 1977 Views
  • 3 replies
  • 0 kudos