STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1443 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 565 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to reasonably use git source control

I'm trying to create process for development with CubeMX/CubeIDE projects.I'm seeing pathing issues that show up when my project is moved. Which also means when it's cloned to another computer.Simple steps I've done to reproduce this:Created a new pr...

0693W00000Dmq5uQAB.png 0693W00000Dmq6JQAR.png

Resolved! Is there a panel to shown warnings in STM32CubeIDE?

HelloI'm using 'STM32CubeIDE 1.7.0'.I've copied a project using: The new project failed the first time I built it as the User Code in main.c had not been copied over. Once I added this missing code the project compiled and ran correctly on the Nucleo...

0693W00000DneRqQAJ.jpg 0693W00000DneRvQAJ.jpg
ron_w by Associate III
  • 3459 Views
  • 2 replies
  • 0 kudos

Must reconnect Nucleo to USB in order to run code

I have a simple cubemx generated project where i simply toggle led and printf to my external console. After programming the program isnt running. i must reconnect the st-link usb interface and then the program will run normally. Simply pressing re...

Rshaw.1 by Associate II
  • 2510 Views
  • 4 replies
  • 0 kudos

Resolved! Intermittent Break at address "0x1fff51f4" with no debug...

Hardware:MCU: STM32L4R9ZGJ6 (Custom board)OSPI mapped to address 0x90000000ST-Link V2PH3-BOOT0 pin pulled to ground with 10k Ohm resistor.Software:IDE: STM32CubeIDE 1.6.0 (Build: 9614_20210223_1703 (UTC)SDK: STM32Cube_FW_L4_V1.14.0TouchGFX assets are...

DerekR by Senior
  • 22021 Views
  • 42 replies
  • 0 kudos

I'm extremely new to all of this. My goal is to connect 2 to 4 accelerators to a STM32F3DISCOVERY and record an event based on the rising edge of a signal. Any direction on this is much appreciated.

I picked the STM32F3 Discovery board because it has 4 ADCs that can supposedly record data at 5MSPS. I am new so a little direction on example code and which pins to use would be great. Im currently trying to be more familiar with the STM32CubeIDE...

MHawk.1 by Associate II
  • 3561 Views
  • 7 replies
  • 0 kudos

Placing string in a fixed memory address on flash

I want to place a variable at a fixed address on my flash memory:#define MYDEF "abcdefg" const u8 MY_CHAR[] __attribute__((section(".ARM.__at_0x0blabla"))) = MYDEF;this works with KEIL IDE, but I switched to STM32CUBE IDE and it is not working. The ...

DGo.1 by Associate II
  • 9713 Views
  • 7 replies
  • 0 kudos

Does the CubeIDE have the 'go' function in the debug mode?

Hello,In the debug mode,after step by step debugging(step over or step in)if I want to run the code from that step, not from the first step of my code,which function could I use?In case of the IAR, 'go' function is provided for this debugging.Thanks.

Kim.Andy by Associate III
  • 1105 Views
  • 1 replies
  • 0 kudos