STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 561 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE 1.1.0 don't start on a Mac OS.

FileVault can't open check the application : "STM32CubeIDE.app is damaged and can't be open. You should placed it in garbage" (translated from french, don't sure all the world in english MacOS).Mac OS 10.14.5.I've the admin right and I can install, i...

0690X00000AsNLoQAN.jpg 0690X00000AsNLtQAN.jpg
jihzed by Associate II
  • 6793 Views
  • 14 replies
  • 0 kudos

Hi, I am using STEVAL-STLKT01V1 and NUCLEO-F303RE and need to run AudioLoop from ac6 System Workbench for STM32 Project. I imported the code and run it but I am getting this error: No source available for "main() at 0x8004304" What can I do?

This is what I have: The system works fine with DataLog. The problem is when I run AudioLoop. What I see is that the COM port is enabled with DataLog and then I run Putty and see the results in real time. However, the COM port is never enabled when I...

0693W00000FATePQAX.jpg
ARami.2 by Associate II
  • 777 Views
  • 0 replies
  • 0 kudos

Resolved! STMCubeIDE 1.7.0 configuration frozen

I have a project created by STM32CubeIDE 1.7.0. Its now impossible for me to change the device configuration, e.g. adding a new peripheral or change anything in a defined peripheral. The device configuration seems to work, but the code generator does...

EDoro.1 by Associate
  • 961 Views
  • 1 replies
  • 0 kudos

Resolved! Elf created but STM32CubeIDE cannot find

Hello I've created a project that has created an elf file: However, when I run debug on STM32CubeIDE I get the following message: Can anyone advise, please? I've not had this problem before with STM32G071, but am trying with STM32F413.Thanks

0693W00000F9xT5QAJ.jpg 0693W00000F9xTFQAZ.jpg
ron_w by Associate III
  • 4749 Views
  • 3 replies
  • 0 kudos

Does STM32CubeIDE generate a target arch macro?

I'm looking for something like __TARGET_ARCH_6_M or __ARM_ARCH_6M__ from my G0 project but don't see anything. Is this done by the IDE based on the selected target hardware, or would I need to add a preprocessor macro manually to my project?

Konami by Senior II
  • 1072 Views
  • 2 replies
  • 0 kudos