STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1422 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE v1.8 and Live Expressions

Please, help me to fix this problem: when I debugging STM32 MCU with J-Link in STM32CubeIDE v1.8 it is not possible to change the Live Expressions tab values 'on the fly' (while MCU is running). The error message is on the pic.

ivainc by Associate III
  • 7920 Views
  • 5 replies
  • 0 kudos

Remote debugger

Hi,I'm looking for a solution to debug a device with remote access.Meaning, the device and an emulator will be in location A and code project will be in a location B. It's prohibited to run the code project IDE on the location A.Device uses STM32F4.A...

ari_v2 by Senior
  • 1318 Views
  • 2 replies
  • 0 kudos

STM32F768I-DISCO unable to run or debug

So I recently purchased an STM32F768I-DISCO board and every time I try to run or debug a code, I get "The selection cannot be launched, and there are no recent launches�?. I do not get any build errors so it I believe it has something to do with the ...

JTurn.2 by Senior
  • 1489 Views
  • 2 replies
  • 0 kudos

hard fault error occur

I use the STM32F100RB and make a bootloader.​The PC is connected to the STM32F100RB via UART, and the program to be executed is sent from the PC and extracted to the internal RAM. However, when the program is executed in the RAM, hard fault error occ...

0693W00000Hp8YVQAZ.png
Myasu.1 by Senior
  • 1156 Views
  • 2 replies
  • 0 kudos