STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1419 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F030F4P6 USART transmit is not happening correctly

Hello folks,I've been started learning STM32 uC and doing UART implementation using HAL library. In this I could see the the transmitted data is received in my tera term terminal, but it is not the one which is transmitted from the code. My code is b...

0693W00000Hq5z6QAB.png 0693W00000Hq5zkQAB.png
PB.4 by Associate II
  • 2905 Views
  • 4 replies
  • 0 kudos

Resolved! Where to check final binary size on CubeIDE1.8.0?

Hello, I want to know final binary size after build like IAR.Currently final output os CubeIDE is Elf file, so I do not know what size it is.(When I use IAR, It showed final binary size on terminal and could also generate binary file.)Is there anyone...

Tiel by Associate II
  • 3412 Views
  • 2 replies
  • 0 kudos

Resolved! Problem uploading code in custom board.

Hi I designed a custom board based on the STM32G030K8 MCU, I was able to upload my code on the device successfully and the device was working fine, I updated the code a few times and was able to successfully upload the code to the board. However I di...

0693W00000Hq06NQAR.png
APant.1 by Associate II
  • 3764 Views
  • 4 replies
  • 0 kudos

STM32Cube. Fail to start GDB server

When I try to flash the stm32G pops up the error "fail to start GDB server.Looking on internet.I have found in the form that a cos.of this error could be Avast antivirus, but even if i have uninstalled it, does not solve my issue.​

FTrom by Associate II
  • 832 Views
  • 0 replies
  • 0 kudos

LWIP over USB with stm32CubeIDE

Hi,Create an http server using ETH and LWIP middleware is easyI would like to use LWIP but using USB_OTG.Do you plan to implement such solution, or does it exist an example of implementation ?Thanks