STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 559 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

hard fault error occur

I use the STM32F100RB and make a bootloader.​The PC is connected to the STM32F100RB via UART, and the program to be executed is sent from the PC and extracted to the internal RAM. However, when the program is executed in the RAM, hard fault error occ...

0693W00000Hp8YVQAZ.png
Myasu.1 by Senior
  • 1159 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeIDE after installing on debian is nowhere to be found

It is Debian based distio (crunchbang plusplus), after installing IDE using sh script provided, the IDE is found in the list of programs, but it is not in the PATH, and I could not find location of the installed files. Also attempting to run installa...

TMark.14 by Associate III
  • 3751 Views
  • 4 replies
  • 0 kudos

Hi, I hope I hit the correct subforum. I cannot update STM32CubeIDE to version 1.8.0. When trying to update, I get the following error message:

An error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).No repository found containing: osgi.bundle,com.st.stm32cube.common.mx,...

AAnth.1 by Senior
  • 1573 Views
  • 2 replies
  • 0 kudos

Cannot import System Workbench project

Project works in System Workbench for STM32 - Version: 1.17.0.201812190825When attempting to import into STM32CubeIDE Version 1.7.0, this popup appears:OK, fine - I pick the correct MCU.Then the same popup appears...At this point, it doesn't matter i...

0693W00000Dm3IQQAZ.png
inojosh by Associate III
  • 3116 Views
  • 6 replies
  • 0 kudos

Resolved! How do I debug an externally built executable?

I built an elf executable for the STM32H743ZI. I did not create this executable from within STM32CubeIDE. Still, I would like to debug it from within STM32CubeIDE. How do I load the elf file in the STM32CubeIDE and debug the executable on a target (S...

AIsma by Associate II
  • 7889 Views
  • 5 replies
  • 0 kudos

STM32IDE: Don't open source when stopping debugging session

This maybe a silly question, but is it possible to set the IDE NOT to open the source file when stopping or pausing a debug session.Nine times out of ten, it stops in a core routine and one just ends up with lot of open files that are generally of li...

AJJ by Associate II
  • 2327 Views
  • 2 replies
  • 0 kudos

Where do I download the GNU Tools for STM32?

This reply to this post claims there used to be a way to download this, but now ST removed the ability to download their patched toolchain? https://community.st.com/s/question/0D50X0000BQOoj5/difference-between-the-toolchain-gnu-tool-for-stm32-and-gn...

Jb.161 by Associate
  • 4274 Views
  • 1 replies
  • 0 kudos

Errors in the configurator of the STM32CubeIDE for microcontroller STM32L100RB. (Not observed for STM32F103, etc.) (Low Layer only)

Ubuntu STM32CubeIDE 1.8/1.7File -> New -> STM32 ProjectChoose STM32L100RB -> Next -> Project Name : "removeMe2" -> FinishIn Device Configuration Tool:  Pinout&Configuration -> Connectivity -> SPI1 -> Mode: Full Duplex Master  Project Manager -> Advan...

ATret.3 by Associate III
  • 2619 Views
  • 1 replies
  • 0 kudos