STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1409 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How do I add checksum to hex image in CubeIDE?

I whish to make a main application for use with a custom bootloader.The main application should be compiled to a hex file with all empty space above the app, filled with 0xFF and with some of the last bytes containing a checksum of the app image.I fo...

0693W00000UnoIXQAZ.png
FwMaker by Associate II
  • 2606 Views
  • 1 replies
  • 0 kudos

How Correctly COPY a Project?

After Pasting one Project, and allowing Uptading Reference Button, I tried to open the *ioc file which issued "error". Then, I had to rename to the newest Project name, then I was abble to open the *.ioc file. So, I might ask: Is it the correct "proj...

JSILV.2 by Senior
  • 1824 Views
  • 4 replies
  • 0 kudos

Resolved! code generation for Keil IDE

Hi , After pin selection and configuration when I try to generate code for keil it does not allow me to change the IDE in project setting, how can I do that?

0693W00000Uo0jLQAR.png
RS009 by Associate III
  • 1818 Views
  • 2 replies
  • 0 kudos

An issue about the blinking text editor

Hi!There seems to be something wrong with m newly installed SMT32CubeIDE. When my mouse cursor moves in the text editor area, it will "blink": Its content disappears for a while and then recover. In the attached two screen snapshots of STM32CubeIDE, ...

0693W00000UnvHWQAZ.png 0693W00000UnvGsQAJ.png 0693W00000UnvHqQAJ.png
OChen.1 by Associate II
  • 2820 Views
  • 3 replies
  • 0 kudos