STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1410 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to build headless inside a docker container

I've installed STM32CubeIDE inside a docker ubuntu image.If I start my docker-image and mount the folder with my source code (base directory is called 'primary' and hostmachine is a MacBook), and run this command:/opt/st/stm32cubeide_1.10.1/stm32cub...

JAnde.15 by Associate
  • 1417 Views
  • 1 replies
  • 0 kudos

Ethernet not working

Hello community, I'm usingSoftware:-STM32CubeIDE v1.10.1--STM32Cube FW_F4 V1.27.1Hardware:-STM32F4Discovery-PHY DP83848-RJ45I want to implement the Ethernet peripheral in the STM32F407 mcu with RMI mode without RTOS (via polling mode), and I used stm...

QSDFG.1 by Associate
  • 1144 Views
  • 0 replies
  • 0 kudos

[SOLVED] Pin triggered Timer-Delay (STM32G4 Timer2)

Hello,how do I have to setup the timer-2 so it create an one-shot delay on every rising edge (could also be falling, does not matter).This timing diagram indicates what I like to do, so I get an output-Event for the DAC and callback for an ISR(option...

0693W00000UoRIRQA3.png 0693W00000UoRIqQAN.png

Resolved! Unable to update STM32IDE

Hi, i cannot update the STM32IDE firmware. I only get this error after a long time of being stuck in the update process at 36%

0693W00000UoGUlQAN.png

Complementary PWM issue

Hi there,I am generating 250khz PWM signal using STM32f401ccu6 (Blackpill) to drive high side and low side mosfets. I am using Timer 1 channel 1 along with its complementary PWM feature to utilize dead time feature. Currently I have generated the PWM...

0693W00000UoJxHQAV.png 0693W00000UoJxMQAV.png 0693W00000UoJxRQAV.png 0693W00000UoJxWQAV.png
Hari123 by Associate
  • 5399 Views
  • 4 replies
  • 0 kudos

Developing in CubeIDE on network drive - corruption.

I was initially getting away with developing on a network drive.However it has all started to come apart.If I attempt to create a new project while the %HOME%\STM32Cube\Repository is on a network drive I get things like "Unable to unzip firmware..."W...

PCamp.2 by Associate III
  • 3076 Views
  • 5 replies
  • 0 kudos