STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1409 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Data with stm32 dma SPI does not flush?

 I'm using HAL with stm32 (H735) and I use SPI5 and SPI4. Both are set up for DMA transfers. The SPI5 works fine and returns data from peripheral to ram. The data out is static, so all good. SPI 4 has changing data out but its not changing. Seems it ...

ulao by Associate III
  • 1373 Views
  • 1 replies
  • 0 kudos

STM32H745 run two tasks simultaneously

I want to run two tasks simultaneously using STM32H745 Nucelo Board. Since it has two cores I think it should be possible. But how should I implement it? Do I need to use FreeRTOS? Is there any documentation/video which I can use to setup two cores t...

AKhot.1 by Senior
  • 1170 Views
  • 1 replies
  • 0 kudos

STM32F411 as usb video input

I built a project, i'm gathering data from an I2C sensor and display the result on a 2.8" tft screen (connected on SPI)since STM32F411 has native USB module, i'm want to let the PC recognize the STM32F411 as a webcam (or any video input device)Any he...

interfacing st4sim-200m with stm32f103 nucleo-64 board

Regarding the  serial communication protocol that I need to use to read and write the data from the module as the st4sim_200m has only one serial I/o port.in the datasheet it is mentioned that to use SPI . but i not able to find the spi peripheral's ...

KKIRA.1 by Associate
  • 960 Views
  • 0 replies
  • 0 kudos

Resolved! Structure of STM32_USB_HOST_Library

Hi,I'm looking to understand the core of the USB Host library, so I thought of trying to update an old project (See: BTstack Port for STM32 USB for details), from the time when there was no STM32CubeIDE (as demonstrated here).The project was created ...

ethernet communication between stm32h745 nucleo boards

Hello everyone, i want to send ethernet packet from one stm32h745 nucleo board to another board. i connect the boards with rj45 biderictional cable, and i use the eth in both boards(one to transmit and one to transmit). i try to debug the program of ...

Ilay2002 by Associate
  • 2553 Views
  • 1 replies
  • 0 kudos

Resolved! Why is SWV not working but my serial monitor is?

I'm running CubeIDE version: 1.12.1 on an Apple Mac (OSx).My board is a STM32f769i-DISCO.I've configured the code as given in numerous examples and I can printf() without issue to an external serial port monitor. The serial monitor is one integrated ...

SFent.3 by Associate II
  • 5802 Views
  • 9 replies
  • 0 kudos