2022-10-28 3:58 PM
Hi, I see the stm32cubeide calls st-link_GDB_server binary program included with the IDE.
I can't find the source code for this program which is based on GDB ( GPL). I checked the St GitHub repos and I was unable to find it.
The st-link project includes other binaries like st-util but not the GDB server.
Any idea where that code is published?
2022-10-31 2:12 AM
Hello @EGho.1
The ST Link GDB server is a proprietary software under ST software license.
You are right that GDB client is under GPL but there is no contamination in between client and server.
No plan to publish ST Link GDB server's code in GitHub.
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.