STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1407 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32CubeIDE - SWV Profiling

Hi,I use the SWV Profiling tool quite a lot towards the end of my projects to "fine tune" the speed and efficiency of my code. i.e. what code to run from ram, whether to use cacheing, find inefficient algorithms etc.It would be handy to export the Pr...

Snag_e50b894.png

Switching from STM32H743ZIT (2MB) to STM32H743ZGT (1MB)

We need to start building with the 1MB STM32H743ZGT while all the development has been done for the 2MB STM32H743ZIT.  As far as I can tell I cannot change the micro in the .iot file for file generation even though the pin assignments and peripherals...

PFlor.2 by Senior II
  • 1875 Views
  • 2 replies
  • 2 kudos

Resolved! Adding a file (Inc)

Somehow I'm blinded at the moment. How do I simply add a file from the filesystem into the project ?I created a header file "times.h", put it into ~/STM32CubeIDE/workspace_1.4.0/project/Core/Inc. Now it sits there. Opening the tree view, I don't see ...

Resolved! Porting STM32CubeMX project to STM32CubeIDE

Hi,I keep getting errors when trying to port a project from STM32CubeMX (v6.9.0) to STM32CubeIDE (v1.13.0). I have updated IDE due to a previous error stating incompatibility between the versions of MX being used - this has now been replaced by the a...

octo-ig by Associate
  • 5116 Views
  • 3 replies
  • 0 kudos

stm32h747i-disco usart1 y usart2

When i use UART at  fp_vision_app.c,why i use usart1 (huart1)the led blue is shinning and the screen show all the information. But when i use usart2(huart2),the led blue is on and the screen get block(nochange) all the setting is the same only change...

wjian2_0-1690208163562.png wjian2_1-1690208198800.png wjian2_2-1690208223656.png
wjian.2 by Associate III
  • 987 Views
  • 0 replies
  • 0 kudos

Change App start address in STM32F4 ( Bootloader USB + App)

Hello all,I have a project using STM32F407 with 1MB of flash and it uses :USB Bootloader project ( start address 0x8000000)App project ( Start address  0x800C000)I want to change the App start address to sector 4 ( 0x08010000)From my understanding I ...

HHich.1 by Associate II
  • 1839 Views
  • 1 replies
  • 0 kudos

STM32L476RG-EVAL, no output to realterm using lpuart

Hello,I have been following a tutorial which is supposed to transmit a string of characters from the board to the realterm terminal on my computer across the USB st-link, however when I run it I do not see anything in the realterm terminal  This is t...