According to the data sheet for this device, I should be able to attached an external High speed crystal instead of using the HSI RC. However, I can't seem to figure out how to do this using the STM32CubeMX utility.
Does ST manufacturer a chip that allows integration into a project which provides USB to SWD for the additional ST32 chips? I would like to remove the need for an external programmer and just be able to add a preconfigured USB to SWD SW-Link bridge ...
Isn't ATMEL/AVR now Microchip? Away, an STM32F1 can be purchased with ST-LINK/V2 preprogrammed on them? Do they then interconnect to another SWD STM32? Or is the STM32F1 the total package and you have to link your application with the preloaded ST...
I guess I did not state my question clearly. I am aware of standard USB to UART and using boot modes to boot and even program some devices. However, what I was hoping for is an ST chip set that replaces the need for the ST-LINK SWIM external progra...