2023-01-27 5:53 AM
If you try to create a new project via target selection and try to search for the commercial part number, the cursor moves to the search bar immediately below each time you try to type a character.
Details from about page:
Version: 1.11.2
Build: 14494_20230119_0724 (UTC)
2023-01-27 10:42 AM
Welcome, @PMarz.2, to the community!
With which operating system are you running the STM32CubeIDE?
Regards
/Peter
2023-01-31 4:55 AM
I'm running the IDE on Windows 10 build 19045.2486
2023-01-31 5:00 AM
What is the complete path name of the directory where you installed STM32CubeIDE?
What does the command java -version show using Command Prompt?
2023-01-31 5:05 AM
ST path:
C:\ST\STM32CubeIDE_1.9.0\STM32CubeIDE
and java version:
openjdk version "11.0.15" 2022-04-19
OpenJDK Runtime Environment Temurin-11.0.15+10 (build 11.0.15+10)
OpenJDK 64-Bit Server VM Temurin-11.0.15+10 (build 11.0.15+10, mixed mode)
2023-01-31 5:08 AM
For me, when I enter a part number (or a part of it) in the search pane, usually nothing is found. Sometimes it works, but then it appears to be case sensitive. There is definitely a problem with the search feature of part selector in CubeMX.
2023-01-31 5:45 AM
If there was definitely a problem, it would occur with every user and the community would be overflowing with requests. However, I have never experienced such a problem, neither myself nor in customer trainings with a large number of participants.
So it is important to find the cause in each individual case. One idea is a competing Java version that pushes itself to the fore and could cause something like this. Even though in this case the JDK seems unsuspicious, it does not mean that STM32CubeIDE tries to use it.
Perhaps the search path and possible other Java installations should now be checked again.
Regards
/Peter