STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 561 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

AWD on the STM32F3Discovery

Hello everyone, I am new to the world of STM32 and trying to get an AWD going on the STM32F3Discovery, this with no success. I have followed the following guide, https://community.st.com/t5/stm32-mcus/how-to-configure-and-use-the-stm32-s-adc-analog-w...

HP- by Associate
  • 1686 Views
  • 1 replies
  • 0 kudos

How do you change the background colour in STM32CubeIDE?

How do you change the background colour in source code editors? I have tried:Window > Preferences > General > Appearance > Theme set to dark modeWindow > Preferences > General > Editors > Text Editors > Annotations has nothing for the backgroundWindo...

qua by Senior
  • 14969 Views
  • 12 replies
  • 1 kudos

Hard download link for STM32CubeIDE

Hello,I am currently scripting my development environnment setup on windows in order to facilitate the setup of a new environnment.For the download of the stm32cubide software, I notice that the download link of the software is not the same for each ...

Clément by Associate
  • 1969 Views
  • 1 replies
  • 0 kudos

Resolved! System clock restore to default

Hello,I need to restore the system clock to its default state, after it has been configured to generate 64MHz clock signal from an external 24MHz oscillator.I used the HAL_RCC_DeInit() function, that seems to do most of the job, but not all apparentl...

CTabo.1 by Senior
  • 3748 Views
  • 5 replies
  • 1 kudos

STM32L476 + ST25RU3993

When I tried to start my device using the sample code provided by the manufacturer, I received the error messages "SetBaseFrequency not working" and "PLL not working". I have confirmed that the device's crystal is functioning properly and the MCU is ...

Alex_tw by Associate II
  • 2836 Views
  • 6 replies
  • 1 kudos

Resolved! Upgrade issue IDE 1.10.1. Project to IDE 1.13.1

Hi, I tried to use a broadcom lib (AFBR_S50, libafbrs50_m4_fpu.a)  on a STM32F401 nucleo board.This works quite well for the IDE 1.10.1. I can compile the example program and run the debugger. But as soon as I try to migrate it to a higher IDE versio...

ekopi by Associate
  • 1615 Views
  • 2 replies
  • 0 kudos

Resolved! Toolchain version

Hello,is it ok to use the __GNUC__, __GNUC_MINOR__ and __GNUC_PATCHLEVEL__ marcros, to check the toolchain version, at compile time?I am using the following toolchain version:In this case and the macros have the following values:__GNUC__ = 10__GNUC_M...

CTabo1_0-1694526170625.png
CTabo.1 by Senior
  • 1325 Views
  • 2 replies
  • 1 kudos

Resolved! RTOS use Taskhandle in other .c file

Hello guys,i try to use RTOS with my STM32H723, but i have some trouble with the RTOS Tasks and the proper definition of the task.As an example i want to push the blue button on my Nucleo board, which triggers an Interrupt, which executes a RTOS Task...

DeBa92 by Associate II
  • 2779 Views
  • 1 replies
  • 1 kudos

Failed to start GBD server

Hi everyone, I'm working with the STM32H747i-Disco, had several projects working just fine, then I tried to load the example project FatFs_uSD to the board, it didn't work and after that I keep getting the error: Failed to start GBD Server. Any Idea ...

GDB server.jpg
JuanBT by Associate II
  • 1469 Views
  • 1 replies
  • 0 kudos

Resolved! GCC Linker script sections

How to put all code from one file in one linker section?I'm using Cubeide with gccThe following functionality should work but it doesn't for some reason, can anyone help here?It shall be possible to group functions in a section based on some filters....