STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1400 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 554 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! SPI COMMUNICATION THREE WIRE/ FOUR WIRE

Hi,I have doubt with the spi communication setup in this configuration. I'm using two sensors where one of the sensor only support 3 wire spi and another  is 4 wire .I have a single spi in mcu. The hardware setup is followed by mapping four wire spi ...

Resolved! How to use the SWV statistical profiling menu in stm32cubeide.

I am developing a device using stm32f429zit6. I want to know the usage rate of all software functions in the project, how to use the SWV statistical profiling menu in stm32cubeide? After setting Debug (Trace Asynchronous Sw), debugger menu, and seria...

image1.png image2.png image3.png image4.png
joseph05 by Associate III
  • 3329 Views
  • 1 replies
  • 0 kudos

Resolved! ST-link v2 running on STM32Cube Programmer

I've recently bought a cheap Chinese ST-link v2 clone. It uses a Geehy APM32 MCU. Which is I guess  STM32 clone. I've since replaced it with a genuine STM32 MCU and st-link firmware. I was able to run it on  STM32 ST-link utility. But failed to run i...

stm32 I2c won't send data

I am trying to get to use I2C on my stm32L4R5ZIT-P.i am trying to configure a sensor by sending data but the I2C pins wont give a signal?i dont ude interups or DMAthese are the pins that i use and the setting for I2C: this are the includes i usethis ...

fontys_student_2-1705416583285.png fontys_student_1-1705416526079.png fontys_student_3-1705416909107.png fontys_student_4-1705416964693.png

Resolved! .ELF mismatch issue

If i compile the same source code in different pcs using same STMCUBE IDE version , Whether i will get same .ELF file?In my case, If i do a comparison(using beyond compare),its not matching and there are significant difference between the two .ELF fi...

KJ.4 by Associate III
  • 2041 Views
  • 2 replies
  • 1 kudos

STM32L010 - printf debug

Hello together, I developed a PCB with the STM32L010RBT6 on it and I would like to debug with printf. I connected the SWD Pins (3.3V, SWCLK, SWDIO, GND, NRST) to my Nucleo F446RE kit for SWD debugging. So far so good I can now debug in the CubeIDE bu...

Claus_CE by Associate II
  • 3112 Views
  • 4 replies
  • 1 kudos

STM32CubeIDE "Updating Software" has encountered a problem

While I was running STM32CubeIDE 1.14.0 today I was notified that there were updates available. So I clicked on the alert note and got suggested to update ST32CubeIDE and it ran into an error: An error occurred while collecting items to be installed ...

chriskuku_0-1705483042130.png

Resolved! Reading data from lis3mdl magnetometer with NUCLEO-L412KB

I've been trying to read data from the OUT_X register of the LIS3MDL using a NUCLEO-L412KB, but I'm not getting any meaningful data output. When I move the device around, the output data doesn't change. I've connected CS to 3.3V and SDO to ground. Wh...

mvari by Associate II
  • 5814 Views
  • 4 replies
  • 0 kudos