cancel
Showing results for 
Search instead for 
Did you mean: 

HSE clock configuration for nucleo STM32F429zi board at 80MHz

Dushyantsingh
Associate II
&clk_lsi {
status = "okay";
};
 
&clk_hse {
hse-bypass;
clock-frequency = <DT_FREQ_M(8)>; /* STLink 8MHz clock */
status = "okay";
};
 
&pll {
div-m = <15>;
mul-n = <96>;
div-p = <2>;
div-q = <4>;
clocks = <&clk_hse>;
status = "okay";
};
 
&rcc {
clocks = <&pll>;
clock-frequency = <DT_FREQ_M(80)>; /* highest value to get a precise USB clock */
ahb-prescaler = <1>;
apb1-prescaler = <2>;
apb2-prescaler = <1>;
};

But the above configuration is not working can you please provide any idea on this.
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead III

Hello @Dushyantsingh 

You may take a look at the configuration of HSE bypass in this project.

Best regards.

II

View solution in original post

2 REPLIES 2
Issamos
Lead III

Hello @Dushyantsingh 

You may take a look at the configuration of HSE bypass in this project.

Best regards.

II

Peter BENSCH
ST Employee

@Dushyantsingh it looks like you are using the NUCLEO-F429ZI with Zephyr, right?

However, your settings are not plausible, because with HSE=8MHz and &pll {div-m = <15>; ...} you only get 533.333kHz. The PLLM output frequency must be at least 950kHz. The current values in &pll{} also result in only 12.8MHz instead of 48MHz at output Q of the main PLL. So you should check your settings again with the RM0090 or CubeMX or CubeIDE.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.