cancel
Showing results for 
Search instead for 
Did you mean: 

How to retain unsed constant variables

CTabo.1
Senior

Hello,
I define following constant string, indicating the program version.

static const char version_s[] __attribute__((used)) = "V.10";

This string isn't used in other part of code, but is only defined with the purpose to put in the binary file, a string easy to find, and to make the CRC over the code, depending from the program version.

However, I see that the version string is not included in the binary file, and consequently CRC doesn't depend on it.

Where is the mistake?

Thank you,
Carlo.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Super User

As @Tesla DeLorean wrote - linkers do removal of unused code. Attribute(used) affects only the compiler, you need something else for the linker. For the GNU linker use a custom section with KEEP in the linker script. For IAR, use specifier __root.

View solution in original post

6 REPLIES 6
TDK
Super User

If you use the string to calculate a CRC, it'll be included in the binary. How do you know it's not included? When you calculate the CRC, what data is it using? Perhaps show the relevant code.

 

If you feel a post has answered your question, please click "Accept as Solution".

Hello,
I tried to modify the constant string value, but the CRC didn't changed.
So I tried to search the "V.10" string in the .elf file, using a binary editor, and I wasn't able to find it.

TDK
Super User

It sounds more like a program bug than a compiler/linker issue. If you're using the string in the program, the compiler has to include it. It can't optimize it out since it doesn't know how the CRC functions, and all CRC accesses are volatile.

If you feel a post has answered your question, please click "Accept as Solution".

If you don't reference things internally the linker is apt to apply dead code removal to discard things.

Check .MAP files for the symbol, and perhaps refer to it or use the KEEP() directive in the Linker Script

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Pavel A.
Super User

As @Tesla DeLorean wrote - linkers do removal of unused code. Attribute(used) affects only the compiler, you need something else for the linker. For the GNU linker use a custom section with KEEP in the linker script. For IAR, use specifier __root.

CTabo.1
Senior

Thank you @Tesla DeLorean  and @Pavel A. 

I modified the linker script, adding the new section .ver, with the KEEP directive

.ver :
{
. = ALIGN(4);
KEEP(*(.ver))
. = ALIGN(4);
} >VER

Then I have allocated my constant version string in the new .ver section:

static const char version_s[VERSION_STRING_LEN] __attribute__((section(".ver"), used)) = "V.1";

And now, when I modifiy the version_s[] value, the CRC changes too.

 

Moreover, I have seen that it works also without specifing the used attribute:

static const char version_s[VERSION_STRING_LEN] __attribute__((section(".ver"))) = "V.1";

In this last case, however, I have the following warning:

warning: 'version_s' defined but not used [-Wunused-const-variable=]

So I prefer to specify also the used attribute.

 

Thank you,

Carlo