STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1467 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 570 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Build issue - error directive usage

Hi All, I am having a strange error. When I compile my code, the error directive causes the ERROR. I can not pinpoint the issue. Could you please hint me in the right direction?Thanks and Regards,  

demir_0-1706300477525.png
demir by Senior II
  • 1615 Views
  • 2 replies
  • 2 kudos

Resolved! Conversion of int to float and float to int

Hello guys, I hope you're doing well, I'm currently trying to replicate a video I saw on YouTube about audio processing using stm, I'm just starting to develop for stm and I'm having some doubts, mainly in terms of libs. I'm trying to convert between...

STM32L072 LIN Communication

Hello everyone,I currently facing an issue. I can successfully send the break and sync byte, but for some reason, my ID is not being transmitted. When I switch from RDR to TDR in LIN_UART_ISRHandler, I can receive all the data from slave on the Picos...

Ofaro.1 by Associate II
  • 1427 Views
  • 0 replies
  • 0 kudos

Accuracy of internal RC oscillator of STM32F030C8

Hi ST Community,I am planning to design a board with STM32F030C8 that will be mass produces. It will be very small PCB, so I am plannig to use internal RC oscillator of the MCU. The MCU will use I2C1  (to write some data to LCD with I2C converter) an...

shydv15 by Associate II
  • 1858 Views
  • 1 replies
  • 2 kudos

Resolved! Include files help.

I have a source folder named components where each subfolder has a .c and a .h file, see screenshot below.I am trying to include these files, but they cannot be found. So far, I know that I should add the relative path and so I did. (I also tried to ...

ubaldot_0-1706174213811.png
ubaldot by Senior
  • 2725 Views
  • 2 replies
  • 1 kudos

STM32CubeIDE 1.13.1 and STM32CubeMX 6.9.1 released.

STM32CubeIDE 1.13.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.9.1 that is available for download.Main issues fixed in this patch:This patch release fixes the issues related to the following cases:STM32CubeM...

Resolved! USART configuration problem

Version: 1.14.1MCU package: STM32CubeF1 Firmware Package V1.8.0 / 26-June-2019The GPIO Settings of the USART auto configuration are incorrect.

Shiina_0-1706153797998.png
Shiina by Associate III
  • 2244 Views
  • 2 replies
  • 1 kudos