Skip to main content
Freedom_Neo
Senior
March 9, 2022
Solved

error: unknown type name '__root'

I am using below codes. But this define not supportted

#define KeepInCompilation __root

0693W00000KbyTvQAJ.png 

#define KeepInCompilation __root
 
/* Private function prototypes -----------------------------------------------*/
int Init ();
KeepInCompilation int Write (uint32_t Address, uint32_t Size, uint8_t* buffer);
KeepInCompilation int SectorErase (uint32_t EraseStartAddress ,uint32_t EraseEndAddress);
KeepInCompilation uint64_t Verify (uint32_t MemoryAddr, uint32_t RAMBufferAddr, uint32_t Size, uint32_t missalignement);
KeepInCompilation HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority);
KeepInCompilation int MassErase (uint32_t Parallelism );

This topic has been closed for replies.
TDK
TDKBest answer
March 9, 2022

> #define KeepInCompilation __root

Why is this here at all?

After some searching, appears to be a macro for the IAR compiler. STM32CubeIDE uses GCC.

https://github.com/search?q=KeepInCompilation&type=code

Appears to be code that was blindly copy/pasted without the necessary #if statements.

https://github.com/chcbaram/stm32_ext_flash/blob/9724a4d5e393c3e84b7b190fcebe4269b21f5d2e/stm32h750_ext_flash_W25Q128FV/src/ap/Loader_Src.h#L20

"If you feel a post has answered your question, please click ""Accept as Solution""."

11 replies

TDK
TDKBest answer
March 9, 2022

> #define KeepInCompilation __root

Why is this here at all?

After some searching, appears to be a macro for the IAR compiler. STM32CubeIDE uses GCC.

https://github.com/search?q=KeepInCompilation&type=code

Appears to be code that was blindly copy/pasted without the necessary #if statements.

https://github.com/chcbaram/stm32_ext_flash/blob/9724a4d5e393c3e84b7b190fcebe4269b21f5d2e/stm32h750_ext_flash_W25Q128FV/src/ap/Loader_Src.h#L20

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
March 9, 2022

Yes would typically be in an include file,

Whoever wrote this code must have had specific assumptions about the tools they were using, people lifting the code need to be aware of the tools that were used, and there exceptions, and adapt the code to work with their own tools, or use the more flexible definitions where it identifies a sub-set of common tools, and provides the appropriate directive.

The reason you need to "Keep" the entry points is that they aren't called internally, but need exporting externally as the loader is pulled in a bit like a DLL, and has multiple entry points, and isn't using main(), or the C run-time initialization methods.

I tended to deal with this at the Linker Script level

https://community.st.com/s/question/0D53W00000SbsggSAB/generating-external-loader-stldr-for-specific-hardware

https://community.st.com/s/contentdocument/0693W000006HJN7QAO

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TDK
March 9, 2022

How do you call them if they're not called internally and aren't at fixed memory addresses? I guess you could examine the map file, but that seems awkward at best.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pavel A.
September 21, 2023

"KeeInCompilation" macro is a misnomer. The intent is to keep the thing in the final image (after linking - not compilation!)

How this is implemented depends on the toolchain. For the IAR compiler this should be defined as "__root" and it is somehow passed to the linker. The GNU compiler knows attributes "used" and "unused" but these do not propagate to the linker (or the linker ignores them, I don't know). So for GNU toolchain, we change the linker script and define KeeInCompilation as nothing (better rename it to something more appropriate).

Senior
September 21, 2023

Pavel A. thank you for the quick respond. I'm not a specialist when it concerns linker files.
You wrote: "So for GNU toolchain, we change the linker script and define KeeInCompilation as nothing (better rename it to something more appropriate)."

Could you please provide me an example code as the one you have described? I use STM32Cube IDE 1.11.2. Everywhere where "KeepInCompilation"is stated in stm32CubeIDE i have deleted it, it gave me errors in my code. When i deleted it,my error dissapeard. But i don't know if deleting "KeepInCompilation" would be the cause of my external loader not working properly in STM32CubeProgrammer.  I try to make an external loader, but have some errors in STM32CubeProgrammer.

Pavel A.
September 21, 2023

@FLuba.1 Examples were pointed by Tesla earlier in this and other threads. Basically you (a) put the needed functions in a custom section and (b) define this section in the linker script, in appropriate place, with attribute KEEP. This tells the linker not to discard that code as unused, AND place the code in specific way. But problem in your loader can be caused by something else. What exactly it is? Post a new thread, please.

Tesla DeLorean
Guru
September 21, 2023

As I said, I address this in the Linker Script, by establishing the symbols I want to retain and export.

https://github.com/cturvey/stm32extldr/blob/main/ExternalLoader.ld#L43

Whereas KeepInCompilation is a tool chain specific macro to flag to the linker, by way of the compiler, that a function is used somewhere, and thus not subject to dead-code-removal. You can check the exports/symbols with tools like objcopy or fromelf

 

#ifdef __ICCARM__ // IAR
#define KeepInCompilation __root
#elif __CC_ARM // MDK-ARM V5.xx
#define KeepInCompilation __attribute__((used))
#elif __clang__ // MDK-ARM V6.xx
#define KeepInCompilation __attribute__((used))
#elif TASKING // TrueStudio
#define KeepInCompilation __attribute__((used))
#elif defined(__GNUC__)
#define KeepInCompilation __attribute__((used))
#endif

 

ST has some specific expectations with .ELF / .STLDR object files. Typically they are not going to use main() and an entry point, there's not startup.s code to clear or move static initializations, and there's no expectation of an interrupt vector table. The StorageInfo struct has specific size, content and placement expectations too.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Senior
September 22, 2023

Thanks a lot.