STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1553 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Not able to see my project in STM32CubeIDE

Hello all,I have created a project using STM32CubeIDE in my memory stick and I was working with it for while with no problem. Then I had to change my work space to somewhere else and now when I want to reopen that project, STM32CubeIDE doesn't show i...

BMano by Associate II
  • 7926 Views
  • 4 replies
  • 2 kudos

Resolved! Power Consumption STM32

Hello everyone,I need to get some information about the power consumption of the STM32 Nucleo-64 with STM32F401RE MCU.The board is powered from the computer's USB port.I created a project in which the main while loop is empty, all peripherals are dis...

RTC output crazy setting ?!

I've spent hours searching and debugging why PC13 is "broken", almost gave up.The reason is that the setting in stm32cubeide says on RTC-output is disabled, but still it's on PC13.-This has to be set as "no RTC output" ! Now it's "disabled" or whatev...

MAalt1_0-1712594297936.png MAalt1_1-1712594440183.png
MAalt.1 by Associate
  • 739 Views
  • 0 replies
  • 0 kudos

Prebuild Command Variables in STM32CubeIDE

Hi,I have a prebuild.sh expecting two inputs from the environment. I also have a script.bat that curls in these two inputs, for the prebuild.sh. I linked these two scripts via && in the prebuild command step setting in the IDE. In the build steps com...

DLin3_0-1712588850537.png
DLin.3 by Associate II
  • 1417 Views
  • 0 replies
  • 0 kudos

USB Access

When secure manager is installed, USB is not working. Can you share me the process to activate USB. when secure manager is installed

Hitesh by Associate III
  • 6255 Views
  • 12 replies
  • 5 kudos

NexDuo MQTT Example

Good dayI downloaded the STM32CubeH5-main folder from github. I am using the STM32H563 Processor and need to get MQTT working. It is a custom board and I already managed to import exampled from ST (using "Import STM32Cube example" option).I susccessf...

SDu T by Associate III
  • 1924 Views
  • 2 replies
  • 0 kudos