User Activity

After downloading en.x-cube-matter-v1-0-3.zip and attempting to install from a local folder, as CubeIDE 1.14.1 nor 1.15.1 have it listed as a package yet.It asks for the .zip or .pack file, shortly after selecting the zip file I get the message as in...
Netxduo packet pool is using 51K, plenty I would have thought to download a 16K test file.This problem was initially seen on an F417 board, and then an F429, so moved on to an H723, specifically the NUCLEO-H723ZG.I filed a bug report at https://githu...
Microsoft's netxduo is at version 6.3.0 released 23rd October 2023 see  https://github.com/azure-rtos/netxduo/releases/tag/v6.3.0_rel The STM32H7 netxduo is at 6.2.0, committed on 5th April 2023 https://github.com/STMicroelectronics/x-cube-azrtos-H7/...
This initially an azrtos tx toggle LED test on a STM32F4Discovery boardI followed this videoMOOC - Azure RTOS workshop - 5 ThreadX lab - step1 - First thread creation - YouTubeThe attached fileSTM32F4DISCO-1.10.1 works when compile with 1.10.1After f...
Below Quoted from: lwIP - A Lightweight TCP/IP stack - Summary [Savannah] (nongnu.org)lwIP 2.1.3 released     posted by goldsimon, Wed 10 Nov 2021 06:52:43 PM UTC - 0 replieslwIP 2.1.3 is now available from the lwIP download areaor via git (using the...
Kudos given to