STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1407 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

USB Access

When secure manager is installed, USB is not working. Can you share me the process to activate USB. when secure manager is installed

Hitesh by Associate III
  • 6087 Views
  • 12 replies
  • 5 kudos

NexDuo MQTT Example

Good dayI downloaded the STM32CubeH5-main folder from github. I am using the STM32H563 Processor and need to get MQTT working. It is a custom board and I already managed to import exampled from ST (using "Import STM32Cube example" option).I susccessf...

SDu T by Associate III
  • 1877 Views
  • 2 replies
  • 0 kudos

library and example experience comparible to the Arduino IDE

I had my first introduction to the STM32Cube and ST MCUs ecosystem and i'm trying to create applications that go further than blinking a led.In the Arduino eco system, when playing with stepper motors, an SPI temperature sensor or even ethernet stuff...

sumbals by Associate
  • 3545 Views
  • 4 replies
  • 0 kudos

TFCard SDIO HAL_SD_ERROR_REQUEST_NOT_APPLICABLE

STM32Cube_FW_F1_V1.8.5STM32CubeIDE:1.13.2MCU:STM32F103RCT6problem description::::::::SDIO-------- f_mkfs((TCHAR const*)SDPath, 0, 0) or f_open(&SDFile, "STM32.TXT", FA_CREATE_ALWAYS | FA_WRITE|FA_READ) [ff.c 4170] ---->stat = disk_initialize(pdrv);[d...

STM32CubeIDE 1.12.1 / Ubuntu 23.04

Hello!I have a problem installing STM32CubeIDE 1.12.1 over Ubuntu 23.04. It says it doesn't find libpython2.7. Does anyone know how to install it?Thanks!

PG.1 by Associate III
  • 5834 Views
  • 7 replies
  • 5 kudos

IDE Download error

I encountered with an error that This software is not available for download when I clicked on the get latest button to download the stm32cubeide software. kindly let me know what should I have to do? https://www.st.com/en/development-tools/stm32cube...

Screenshot 2024-04-01 083734.png