Stm32CubeIDE 1.14.0, STM32CubeMX 6.10.0, STM32CubeFW_U5 V1.4.0, X-CUBE-FREERTOS.1.1.0
This started with the Stm32CubeIDE 1.14.0 release and worked fine in 1.13.x. It happens for new projects and migrated projects. I'm using it with an STM32U5.
Go...
How do I import the BSP and OSPI_NOR_MemoryMapped examples from the STM32CubeU5 package for the STM32U5A9J-DK board? That series of board is not listed as supported in the example selector, so I have to use the git repo. These are all examples that...
I am encountering a warning when trying to generate code for both existing and new projects in STM32CubeIDE 1.14.0. This did not happen in 1.13.x. I get the following warning. I have been generating the code and it appears to work, but I don't know...
Does these boards work out of the box with an external debugger like a J-Link Ultra+? I see they both support a MIPI10 connector (and one supports a tag connector as well) that leads me to believe it supports an external debugger. However, I can't ...
If I remember right, you need to move solder bridges to get the SWO output to work. See SB33 and SB34 in the manual and the section "SWD debug/program/trace and JTAG/USART".
I'm using 1.14.0.I tried this method and then when I try to build, I get multiple errors due to not being able to find "stm32u5xx_hal.h"I also notice it references other include directories that are empty, such as the hal_driver and cmsis directories...
Do you need SWO for the JLink to work? I noticed that the SWO pin is not connected by default (solder bridge removed) and the pin is connected to something else. It's on page 39 in um2967-discovery-kit-with-stm32u5a9nj-mcu-stmicroelectronics.pdf