User Activity

I've been using the recently added CMake generation feature of cubemx, as of now it creates an INTERFACE library for both project related and drivers related sources, the problem is that those sources get propagated for every external library that ne...
I don't know if this is caused by the vscode extension or stm32cubeclt, but after the installation(everything related to the extension works), I noticed that the system path variable had been modified to add stm32cubeclt bin directories(I found this ...
I've had this problem for months now, in Debian 12/13(and Ubuntu 20.04), if I suspend my PC while STM32CubeIDE(1.12 to 1.14, both generic linux and debian versions) is running, when I wake up the PC and log in, STM32CubeIDE is completely freezed, I d...
Is STMicroelectronics ever going to partner with Espressif to integrate short distance wireless connectivity with stm32 MCUs? Would this be a good idea? Right now, the only good library that integrates Wi-Fi connectivity and networking in stm32 using...