STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE 1.12.1 / Ubuntu 23.04

Hello!I have a problem installing STM32CubeIDE 1.12.1 over Ubuntu 23.04. It says it doesn't find libpython2.7. Does anyone know how to install it?Thanks!

PG.1 by Associate III
  • 5852 Views
  • 7 replies
  • 5 kudos

IDE Download error

I encountered with an error that This software is not available for download when I clicked on the get latest button to download the stm32cubeide software. kindly let me know what should I have to do? https://www.st.com/en/development-tools/stm32cube...

Screenshot 2024-04-01 083734.png

Resolved! ELF file and converted BIN far too large

Hi  I have an STM32L433CBT processor and created a project using STM32 IDE version 1.14. I created the project on STM32 MX version 6.9.1 .  The project works in debug and I created a release version , but the elf file is far too large. I have the fol...

SSmit13_0-1712322217944.png SSmit13_1-1712322284193.png SSmit13_2-1712322477259.png

Resolved! STM32CubeIDE V1.15.0 H7 series ADC3 Problem.

Hello?As title, at STM32H750, when will be fix to use termperature sensor/vbat/vref? In version 1.15, all checkboxes were cleared. Due to migration, the lower version couldn't even read it, so I reset it from the beginning.And then, it seems that the...

LSung.1 by Associate III
  • 2703 Views
  • 3 replies
  • 0 kudos

comply a product to get UL certified

Hi I am working on a product using STM32H563, which requires to be UL certified.In-order to make my code comply with UL certification, I am planning to follow the below approach:I am planning to create a spatial separation between critical and non-cr...

Riya by Associate II
  • 1007 Views
  • 0 replies
  • 0 kudos

Resolved! Why does this go to error handler?

Hi! I have a code that is supposed to develop CAN-bus communication, but these two functions go straight to error handler. Any suggestions why that might be? for reference I'm using the nucle-l433rc-p board.  

Mr4_0-1711961684256.png
Mr4 by Associate III
  • 11265 Views
  • 13 replies
  • 6 kudos