STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1410 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Board Selection Menu

I need to download and populate the STM32 board selector. Currently in order to select a board, eg: Nucleo series, I will need an internet connection. Is there not a way to download the list and use STM32Cube IDE to select from the downloaded list? T...

techdesk by Associate III
  • 3421 Views
  • 5 replies
  • 2 kudos

Resolved! Variadic functions (like prinf)

Hi community,I wrote the following functionUINT PrintOut(const char* format, ...) { va_list args; va_start(args, format); char buffer[1024] = { 0 }; vsprintf(buffer, format, args); va_end(args); return PrintString(buffer); }No problems at co...

Importing drone firmware into STM32CUBEIDE

Not sure if this is the right place to post but for drone firmware such as betaflight or iNav that run off STM32 MCUs like F4xx, how would one go about importing and using the firmware files inside of CUBE IDE so that firmware itself can be changed a...

ZHama.1 by Associate II
  • 5008 Views
  • 4 replies
  • 3 kudos

Using C++ Builder

STMCubeIDE seems to give endless problems. Since the MX can generate c++ code what is the possibility of using all the generated files in C++ Builder? If This is possible, which files should I look for? Has anyone tried this before or will we just ha...

techdesk by Associate III
  • 6303 Views
  • 10 replies
  • 1 kudos

Help Needed: Migrating from MicroXplorer to STM32CubeIDE

Hey everyone,Hope you're all doing well.So, I'm pretty new to ST Microcontrollers and IDEs. I've got a bunch of projects that I've been working on using MicroXplorer. But guess what? MicroXplorer's now outdated. So, I've got to move everything over t...

LuciferD by Associate II
  • 4880 Views
  • 8 replies
  • 3 kudos

Resolved! linker file

The wizard procedure put in my project this file <STM32U575ZITXQ_FLASH.ld> and this file <STM32U575ZITXQ_RAM.ld>.When is used the first and when the second and where is written in the project which one to use?Because in the linker section, as for Deb...

IVent.1 by Senior
  • 4710 Views
  • 1 replies
  • 3 kudos

STM32F4 libusb-win32 with FREERTOS problem

Hello, I'm using STM32F407VGT board to send and receive data to/from a Nodejs application via libusb. This works correctly when not using freeRTOS, but as soon as i create a freeRTOS task or use any CMSIS function such as  osDelay() the board's usb d...

Resolved! stm32f407 ftp client

helloim using stm32f407vgt6 and cubeide without os.i configured ethernet using cubemx perfectly.now i need ftp client, i cant find proper resources for do this.thanks for your helps.