cancel
Showing results for 
Search instead for 
Did you mean: 

Cube IDE opens files multiple times in multi-executables project

Tobe
Senior III

I have a project, that has multiple executables/uC-Code, that has some common headerfiles. These are opened from  the participating projects-folders. But then the same file is opened multiple times. As one can imagine this brings problems and confusion. The compiler would happily compile with the include directiorys setup in the settings, but Cube shows errors.

Is there a way to have it just open one file?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0