STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1406 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! GPIO pins always high on STM32F405RGT6

Hello!I have an STM32F405RGT6 MCU with a custom PCB. I have some trouble with my GPIO pins as they only seem to be high.  I am using the STM32CubeIDE software and have configured all GPIOs. I having trouble with PA12 and PA15 in particular. See GPIO ...

mathieusteketee_1-1714673847264.png mathieusteketee_2-1714674006691.png mathieusteketee_3-1714674122590.png mathieusteketee_4-1714674305061.png

Resolved! Cant enter into debug mode

I am fresher here for the ST cube IDE i am trying to debug my code but it showing this error msg

Neetu by Associate II
  • 4304 Views
  • 7 replies
  • 0 kudos

Resolved! callback not getting triggered by 1us timer (TIM5)

HI,I set TIM5 up to trigger every 1us (APB1 42MHz) with the below function and I expect HAL_TIM_PeriodElapsedCallback() to be invoked every 1us but that's not the case. How do I make sure that the callback gets invoked properly?My init function:stati...

debug by Associate III
  • 2371 Views
  • 4 replies
  • 1 kudos

configuration

Hi,I now implementing i2c with 1 master (U575ZI-Q) and 3 slave (LK432KC).I confirmed my code. It worked well.but after changed title of the project and deleted some project, it made me confued,, so I made every(1master 3slave) project new. Here is th...

eunni_0-1714758042670.png eunni_1-1714758057098.png eunni_2-1714758125923.png eunni_3-1714758171256.png
eunni by Associate III
  • 6318 Views
  • 7 replies
  • 0 kudos

Resolved! Code Generation - USB OTG HS STM32H723ZGT6

Ran into a issue with a fresh blank project, only USB OTG HS turned on. Computer would recognize the usb device but as soon as I would turn any level of optimization on the computer would no longer detect the usb and show it as connected.  I was able...

stm32l051c8 standby mode

hi all currently i am working with stm32l051c8 , using that i can work with standby mode, its not entering to standby mode, can  u guide me any oneif (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET){__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); // clear the flag /** ...

Resolved! STM32CubeIDE Library issues

Hello, I am trying to use the TensorFlow Lite Micro library for my project in STM32CubeIDE.I have made a folder for the library in my project as shown: I have included the directory for the folder in under the "Path and Symbols" tab:When I simply try...

mathieusteketee_0-1714264556733.png mathieusteketee_1-1714264745926.png mathieusteketee_2-1714264895949.png mathieusteketee_3-1714264973248.png