cancel
Showing results for 
Search instead for 
Did you mean: 

Using I2C1 and I2C2 with HSI

volkan_
Associate II

Hi,

I am planning to use STM32F030C8 in my design without external  crystal. I will use HSI as clock. Can I use I2C1 (PB8, PB9) and I2C2 (PB10, PB11) with HSI? 

 

Thank you for the help,

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Of course you can do that. Unlike UART, I2C has a clock line via which the devices are synchronised.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Of course you can do that. Unlike UART, I2C has a clock line via which the devices are synchronised.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.