STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1407 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Can't download drivers and STM32 Cube IDE from web.

Recently bought an STM32 Nucleo F446RE board. To set it up, I wanted to download the drivers and STM32CubeIDE from the website. However, after logging in, when I click the 'Get the Software' button, it pops up with an error message saying, 'This soft...

YAMIN by Associate
  • 3148 Views
  • 3 replies
  • 0 kudos

Resolved! STM32U0

With the STM32CubeIDE I can't debug a firmware, as always the connection is lost:  Download verified successfully  Target is not responding, retrying...Target is not responding, retrying...Target is not responding, retrying...Target is not responding...

Issue with HR Timer PWM Frequency on STM32

Hello STM Community,I'm encountering an issue with generating a PWM signal using the HR Timer (High-Resolution Timer) on an STM32 microcontroller. My goal is to generate a PWM signal with a frequency of 16 kHz, but I'm consistently getting a frequenc...

led blink project in STM32F401RE

I am using stm32f401re. i am trying to blink the led which is internal one. and i couldn't do it. could you please help me with the project as the project is attached below.

suhfi by Senior
  • 1595 Views
  • 1 replies
  • 0 kudos

Resolved! New project on old board

HelloI am using board NUCLEO-G071RBI wrote for it a code, and all worked well.Now I want to rewrite a new project for the same board, but elementary functions such as PWM output doesn't work. If I run again the old project all works OK again.Someone ...

MichaelR by Associate III
  • 1215 Views
  • 1 replies
  • 0 kudos

STMCube IDE fails to erase memory

Hello everybody. I have a custom board with an STM MCU on it.  This is not the first custom board I use, and all the others are working as expected.This custom board works for a replacement of an identical board which stopped working. This means that...

Resolved! winbond W25Q128JVSIQ external loader problem

i am working with stm32 h750vb and i successfully wrote a winbond W25Q128JVSIQ external loader and it works fine on the cube programmer but when i use the cube ide i found that it successfully erase the external flash before file download and fails t...