STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

TrueSTUDIO and ST-Link V2

Hello! I have an old and huge project developed in TrueSTUDIO v9.2 and I'm trying to debug it using the ST-Link V2 (fw V2J43M28) by SWD interface. But right after "Debbuger connected" message, I've got an error: Failure at line: 13. Error finishing f...

Peaga by Senior
  • 1485 Views
  • 1 replies
  • 0 kudos

Piping data to and from STM32 HW during debug?

I am writing audio DSP applications, and to debug and test them I would like to pipe canned data from my Mac to my STM32 HW, then run either my whole algorithm or selected DSP blocks for unit testing, then send the results back to the Mac to compare ...

AVoel.1 by Associate III
  • 1402 Views
  • 1 replies
  • 0 kudos

Cannot install AI-SENSING pack

I am trying to install the AI-SENSING pack into STM32CUBEIDE V1.0.2.I download the zip file from STM website "en.fp-ai-sensing1.zip" When I go from menu "Manage Embedded Software packages", and I try "Install from local" I get the error:"The given fi...

THey by Associate II
  • 1059 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 dual core connectivity protocol handling

Hello,Could you please help me with handling a same channel I2C protocol between 2 core.I have two devices connected on the same I2C channel(I2C1). I want to run one device on M7 core and another on M4 core. How to handle the communication between th...

HDesa.1 by Senior
  • 6427 Views
  • 11 replies
  • 4 kudos

LoRa Base Station

here I am using P-Nucleo-lrwan3 package. It is working with 433/470 MHz RF . I am trying to connect the gateway with loriot server, But it is not Happening I am Trying Multiple servers and Multiple Regions (eu1.loriot.io ,ap1.loriot.io) frequency reg...

suresh_microvision_0-1718176234017.png

Unable to Program My STM32G0B1

I tested PCB with BOOT_0 is Pulldown to gnd & not Pulldown to gnd & tested with both Stlink-V2 & J-Link Segger Even In Cube Programmer also it was not detected.The MCU In this Board is STM32G0B1CET6 & it was bought in element14, this is the first tim...

Sakthi_Murugesan_0-1712739637083.png Sakthi_Murugesan_1-1712739674040.png Sakthi_Murugesan_2-1712741525235.png

STM32CubeIDE 1.15.1 released

STM32CubeIDE 1.15.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.11.1 that is available for download. Main issues fixed in this patch: Ticket 177978 : Fixed an issue with ST-LINK firmware upgrade concerning th...