STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Missing column header labels

Hello,After installing version 1.15.1 of CubeIDE, the labels in the column headers 'System Core/NVIC/Code generation' disappeared. It's not a big issue, but it's a bit annoying.Look at the below image.

screen.jpg
Xanadu by Associate II
  • 2527 Views
  • 4 replies
  • 0 kudos

Resolved! Defines not changing grayed out statuses

Using STM32CubeIDE 1.15.1.  Running LwIP_Server_socket_RTOS on a Nucleo-H723ZG board.When I change #define LWIP_DHCP to zero my DHCP stuff is not grayed out.  It definitely starts using static IP, I'm able to connect and see the web pages.  I'm used ...

st3ph3n by Associate II
  • 3013 Views
  • 4 replies
  • 1 kudos

Resolved! Skip buildsteps during headless build

Hi, i create a pipeline to compile a cubeide project with the cubeide in a docker container. on azure.the docker container is linux based as i found no solution to do a headless cubeide installation on windows(or is there a way?)in my project setting...

funky by Associate III
  • 3389 Views
  • 5 replies
  • 2 kudos

warning [libusb_exit] device 2.1 still referenced

after starting a debug its directly going to hardfault handleractually here there 2 boards1)stm32l476vgt6 (using jtag to load code in stm32h74zit6)2)stm32h74zit6facing this warninglibusb: warning [libusb_exit] device 2.1 still referencedlibusb: warni...

Screenshot from 2024-06-10 17-29-21.png Screenshot from 2024-06-10 17-29-25.png

Cannot create a new STM32 project on cube IDE

I am trying to create a new STM32 project on cube IDE, after I selected with STM32 project and clicked Next. The application not response.And when I double clicked the STM32 Project button, the error shown as below.Any idea?My computer is windows OS ...

WayWei_0-1717678797584.png WayWei_1-1717678805531.png
-WayWei- by Associate
  • 2086 Views
  • 3 replies
  • 0 kudos

Project Explorer - How to lock

Hi, I have used 2-3 versions of STM32Cubeide and 1 thing that is driving me crazy right now is the project explorer is never consistent, sometimes it's visible sometimes it isn't, sometimes the projects disappear completely, sometimes project explore...

PLee.3 by Associate III
  • 1865 Views
  • 2 replies
  • 1 kudos

Resolved! Why cannot properly see opcodes on memory browser ?

I can see the addresses when I hover over them, but I can't see the opcodes. Is there a setting to fix this or is it broken?  Starting server with the following options:Persistent Mode : DisabledLogging Level : 1Listen Port Number : 61234Status Refre...

Untitled.png