2024-06-06 2:07 PM
Hello!
I have an old and huge project developed in TrueSTUDIO v9.2 and I'm trying to debug it using the ST-Link V2 (fw V2J43M28) by SWD interface. But right after "Debbuger connected" message, I've got an error: Failure at line: 13. Error finishing flash operation. It looks like the STM32_Programmer_CLI from TrueSTUDIO is not compatible with the updated debbuger.
Do you guys know if is there a way to replace the CLI by the new one or even downgrade the ST-Link version?
Thanks a lot!
2024-06-12 3:14 PM - edited 2024-06-12 3:14 PM
Hello @Peaga
Could you share the debug log?