STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

My Cube is broke

I've tried reinstalling, uninstalling, running as root, dozens of other things... just getting these issues regardless of anything I try. As far as operation... it will start, but would bind up at 19% on a build. After reinstalling, it now takes fore...

Frad by Associate
  • 1651 Views
  • 3 replies
  • 0 kudos

Giant plugins folder

The plugins folder at C:\ST\STM32CubeIDE_1.14.1\STM32CubeIDE\plugins is 5.24 GB. It has lots of com... folders, lots of org... folders and lots of .jar files. Some of the folders are referenced among my STM32CubeIDE project Includes, even though the ...

JvdV_0-1720230171006.png JvdV_1-1720230551475.png
JvdV by Associate II
  • 3095 Views
  • 5 replies
  • 5 kudos

Empty FreeRTOS Queue window

As per subject. I can see the tasks but it would be most useful if I can see queue status as a USB task isn't always responsive, and mouse movements are discarded if the queue is full.I have added the 12 or so queues into the registry with the vQueue...

Mike xx by Associate III
  • 2355 Views
  • 3 replies
  • 0 kudos

Resolved! Import project to cubeIDE

Hello, I'm new to STM nucleo boards. Got my hands on the p-nucleo-usb002 usb type c evaluation board. I tried to import the demo projects to cubeIDE and it doesnt seem to build. I'm missing out something. Please help! The project files are as in the ...

Screenshot 2024-06-22 112556.png
kushal29 by Associate
  • 1548 Views
  • 1 replies
  • 1 kudos

Resolved! Problems with pointers on STM32H725ZGT6

HelloGlobal definition of pointers:unsigned int *uIntUtilityTmpP; unsigned int *uIntP_2_UtilityTmp;In a function I would like to initialize them with absolute values:*uIntP_2_UtilityTmp=0x15; *uIntUtilityTmpP=455; uCharUtilityTmp=62; sprintf(print_st...

SMali.3 by Associate III
  • 3028 Views
  • 6 replies
  • 1 kudos