STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! 'used' attribute Appears Ineffective

Hello,According to the manual , "This attribute, attached to a variable with static storage, means that the variable must be emitted even if it appears that the variable is not referenced."In the following code, unreferenced_variable is always discar...

Kier by Associate III
  • 13995 Views
  • 23 replies
  • 5 kudos

Resolved! ADC won't start after Cube upgrade

Hi,I have a project on Nucleo board with STM32U575ZIT6Q. I'm using STM32CubeIDE.My ADC worked fine until i did this:After migration HAL_ADC_Start function returns error.When I generate code I use this setting:What is wierd, is that if I unselect this...

migration.PNG code gen.PNG
S-E by Associate II
  • 3899 Views
  • 8 replies
  • 4 kudos

Resolved! Question regarding STEVAL-EDUKIT01

Hello,I wonder if anyone in the community knows anything about this:I ordered the steval-edukit kit found here:https://www.st.com/en/evaluation-tools/steval-edukit01.html#overview I only got the motor controller. The website claims it is a full kit a...

OJM by Associate
  • 2011 Views
  • 3 replies
  • 1 kudos

STM32 SMBUS giving error

im working on SMBUS for STM32F4 controller, im able to enable one I2C and then add middleware for SMBUS from middleware section, and by opting SM-BUS two wire interface i can select that I2C in SMBUS menu, but after this im generating code and gettin...

_kalpesh_0-1716898615788.png
_kalpesh by Associate III
  • 2812 Views
  • 4 replies
  • 1 kudos

Project not compilable on other computer

Hello dear ST CommunityI have my first real problem, unfortunately.Since we now want to work with multiple people on projects, we have now set up our git cleanly by only sharing the project files (no workspace). However, now I unfortunately have the ...

resea by Associate
  • 2169 Views
  • 2 replies
  • 0 kudos