STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1409 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Import project to cubeIDE

Hello, I'm new to STM nucleo boards. Got my hands on the p-nucleo-usb002 usb type c evaluation board. I tried to import the demo projects to cubeIDE and it doesnt seem to build. I'm missing out something. Please help! The project files are as in the ...

Screenshot 2024-06-22 112556.png
kushal29 by Associate
  • 1510 Views
  • 1 replies
  • 1 kudos

Resolved! Problems with pointers on STM32H725ZGT6

HelloGlobal definition of pointers:unsigned int *uIntUtilityTmpP; unsigned int *uIntP_2_UtilityTmp;In a function I would like to initialize them with absolute values:*uIntP_2_UtilityTmp=0x15; *uIntUtilityTmpP=455; uCharUtilityTmp=62; sprintf(print_st...

SMali.3 by Associate III
  • 2948 Views
  • 6 replies
  • 1 kudos

Resolved! connecting AMT-103-V and STM32-Nucleo-H743zi2

Hello everyone,I'm new to STM32 programming and currently working on a project that involves using the AMT-103-V encoder with an STM32 microcontroller. I would greatly appreciate any help or guidance on how to effectively interface and read data from...

Target not responding, retrying but code is working

Hey everyone!I'm using STM32U083C-DK dev board which has STM32U083MCT6 MCU on it.Using STM32CubeIDE, I tried to put the device in Stop2 mode (one of the low power modes) entire time and when a button is pressed, it wakes-up, Blinks an LED and again g...

RB4020 by Associate II
  • 3371 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H743ZGT6 FLASH.ld error

Hi, I am using MCU : STM32H743ZGT6.When I write the code and build it, I get these errors. So even if I create a new project and build without writing any code, I get the same error.  How do I fix this? Error : c:\st\stm32cubeide_1.10.1\stm32cubeide\...

giwonKIM by Associate III
  • 3363 Views
  • 2 replies
  • 2 kudos