STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

cubeıde close

Hello, after updating cubeide, it started to close automatically. While checking for updates, it gives an error and then the program closes. I uninstalled the program and reinstalled it, but the problem persists. I also updated Java but the problem d...

edramden by Associate II
  • 1561 Views
  • 2 replies
  • 0 kudos

Resolved! Global variable overlaps with stack.

Hi.I am absolute noob with stm32 and i am currently trying to connect GY-GPS6MV2 module to RobotDyn STM32 Mini(STM32F103C8T6).  I have connected GPS module to pins and set up USART1 in asyncronous mode. I have done everethyng according to official ex...

STM32_SP.jpeg STM32_Declaration.jpeg
BigBrick by Associate II
  • 7562 Views
  • 14 replies
  • 0 kudos

Resolved! LED won't blink

Hi,First, sorry if my english is bad, I'm French.I have just bought a NUCLEO F207ZG and I try to blink an LED.When I upload the program, the console output :STMicroelectronics ST-LINK GDB server. Version 7.8.0 Copyright (c) 2024, STMicroelectronics. ...

R0M1 by Associate II
  • 3879 Views
  • 7 replies
  • 1 kudos

Resolved! How do I declare a UART Function in a separate C file?

I have a program that displays the current temperature of a room on the UART terminal and I want to start getting into the habit of separating my functions into their own source and header files, however, I'm running into a couple of problems. Here i...

DRicc.2 by Senior
  • 3791 Views
  • 5 replies
  • 4 kudos

Resolved! I cannot import file in Workspace

I put this folder in the workspace with all the other projects:Now I have to import it as I have always done: file - import - existing projects in the workspaceI cannot press on "finish" 

luke514_0-1722331078448.png luke514_1-1722331217735.png
luke514 by Senior
  • 2911 Views
  • 5 replies
  • 6 kudos

flashing

so i am trying to flash the firmware of web builder onto the board stm32h743zi2, then it is showing me error as  "There is no space on NOD_H743ZI2. You need an additional 168kb to copy these files.NOD H743ZI2Space Free : 8.0KBTotal size : 32.0KB"what...

suhfi by Senior
  • 2068 Views
  • 4 replies
  • 1 kudos