STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32H7 debug dual core

Hi everybody,just some info regarding debug with dual core. 1. In Stm32CubeIde is it possible to debug a NUCLEO board equipped with STM32H755 with the two sessions contemporary alive? (The debugger mounted on NUCLEO board is STLINK-V3)2. Is it possib...

lonejack_1-1702591106479.png
lonejack by Associate III
  • 3474 Views
  • 3 replies
  • 0 kudos

Resolved! Failed to execute MI Command Error

Hy!I'm new to STM32. I'm currently using STM32F103C8T6 board, and it give MI command error (image attached). I have tried using STM32 programmer as well to fix it. Still couldn't. How can i fix this?   

Thenuk__a_1-1721051553812.png Thenuk__a_0-1721051525333.png
Thenuk__a by Associate II
  • 2930 Views
  • 5 replies
  • 1 kudos

Resolved! CMAKE build works only in IDE

Hello,I have successfully created a new cmake project in IDE 1.16. Everything I need works - the project is successfully compiled, the BIN file is successfully run in the MCU:[ 97%] Building C object CMakeFiles/KubergCMAKE.dir/Drivers/STM32L0xx_HAL_D...

JKol by Associate II
  • 3019 Views
  • 4 replies
  • 2 kudos

Project creation startup files

I installed STM32CubeIDE and have been trying to create a project using the STM32F407G-Discovery Board. Upon trying to create a project, the startup code generation file doesn't show up.I get the following pop-ups. I am unable to resolve this issue. ...

Screenshot 2024-07-30 095306.jpg Screenshot 2024-07-30 095337.jpg
anishac by Associate II
  • 2368 Views
  • 4 replies
  • 0 kudos

Problem running Stm32cubeIde

I recently installed Cube IDE. When I create a new project is created a blank workspace and none of the options work! I cant find cubeIDE tag so had to use edesignsuite instead

Prnjl10 by Associate
  • 1017 Views
  • 1 replies
  • 0 kudos

Resolved! 3D vectors in C++

Hi,recently I detected "complex.h" and the float complex data type for C++ project files. Since then dealing with complex numbers got very easy. I would appreciate the same ease of use for 3D float vectors, i.e. I need a float vector data type and th...

DetlefS by Senior
  • 2947 Views
  • 5 replies
  • 0 kudos